Technical FAQs

Ask a Question

Can the 1600A PAF2036 circuit breaker in a EZM11600CB EZ Meter-Pak Main Breaker device be converted to an alternate ampere rating?

Product Application

Product Line:
EZM Metering

Alternate main amperage ratings

The PAF2036 circuit breaker frame provided in the EZM11600CB is supplied with PA21600RC rating columns. The PA31600RC rating columns can be removed and replaced with alternate, lower ampere rated, rating columns:
For 600A ampere rating, use PA2600RC
For 700A ampere rating, use PA2700RC
For 800A ampere rating, use PA2800RC
For 1000A ampere rating, use PA21000RC
For 1200A ampere rating, use PA21200RC
For 1400A ampere rating, use PA21400RC

CTA-ID : 2018287
Was this helpful?
What can we do to improve the information ?