Technical FAQs

Ask a Question

What filler plate is available to fill an unused tenant breaker space in the MPL32225, MPL53225 or MPL64225 Meter-Pak units?

Issue:
Selection

Product Line:
Meter-Pak

Cause:
Selection of accessories

Resolution:
Use two (2) QOFP filler plates for each unused tenant breaker space. 
Was this helpful?
What can we do to improve the information ?