Technical FAQs

Ask a Question

Where is the part number for an XCS safety interlock switch

Issue:
Where is the part number for an XCS safety interlock switch

Product Line:
XCS safety switches - GIC Product

Environment:
US Product

Cause:
Product identification

Resolution:
The part numbers for these units are printed on the side of the unit.  The front cover of these devices will only identify the general family and conformance to various standards.
Was this helpful?
What can we do to improve the information ?