Technical FAQs

Ask a Question

What are the termination provisions for branch neutral conductors for HCWM12SN?

Issue:
Product Features

Product Line:
I-Line Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 29 & 94-1989, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2000 IBC, 1995 NBCC 

Cause:
In order to ensure that there are sufficient branch neutral terminations, it must first be known what is provided as standard.

Resolution:
Branch neutral termination provisions (Al or Cu conductor) for I-Line panelboard neutral assembly HCWN12SN are as follows:
(4) 3/0 - 750kcmil 
(7) #6 - 350kcmil
(9) #14 - #10
(17) #14 - #4
 
Was this helpful?
What can we do to improve the information ?