Technical FAQs

Ask a Question

Do the current ATV32 units support Device Level Ring DLR topology for Ethernet IP?

Issue: 
Do the current ATV32 units support Device Level Ring DLR topology for Ethernet IP?
 
Product Line:
ALTIVAR 32, ATV32
 
Environment:
All serial number

Cause:
N/A
 
Resolution:
The current ATV32 units do not support Device Level Ring DLR topology for Ethernet IP.
Was this helpful?
What can we do to improve the information ?