Technical FAQs

Ask a Question

Is there a drawing for the Nema 3R Speedy D Switchboards?

Issue:
Is there a drawing for the Nema 3R Speedy D Switchboard?

Product Line:
Speed D SWBD

Environment:
O/M

Cause:
Record Drawing

Resolution:
Dwg D11 attached, is generic, in that it shows no individual part numbers for specific Nema 3R enclosed Speedy D SWBDS. It is the only available dimensional cut sheet drawing available at this time
Was this helpful?
What can we do to improve the information ?