Technical FAQs

Ask a Question

Cross Reference for ALCRs (Automatic Load Control Relay Devices)?

What is the availabilty of ALCRs (Automatic Load Control Relay Devices)?
These devices might also be known as Emergency Egress Lighting Control Devices and are specified by UL 924 standard.
Is there a cross reference?

Product Line:
Schneider Electric Lighting Control Devices

North America
Commercial Building Lighting Control

As of March 1 2015, Schneider Electric made an exit from this marketed and made its ALCR devices obsolete.  

The original manufacture of the Schneider Electric ALCR devices is LVS Controls.  The same products can be purchase through LVS.
SE Catalog Number LVS Controls Model Numbers Product Description
SLSEDC120 EPC-D-F-S-120 UL 924 120V Emergency Dimmer Control 
SLSEDC277 EPC-D-F-S-277 UL 924 277V Emergency Dimmer Control 
SLSEPMC120 EPC panel mount 120 UL 924 120V Emergency Panel Mount Control 
SLSEPMC277 EPC panel mount 277 UL 924 277V Emergency Panel Mount Control 
SLSERC1277 EPC-A-1 UL 924 120-277V Emergency Relay Control 

Note that the Panel Mount  SLSEPMC120 and SLSEPMC277 are not publically shown on the LVS website.  Those models were made special for Schneider Electric.  They can be ordered by request.
Was this helpful?
What can we do to improve the information ?