Technical FAQs

Ask a Question

Will CM/R work with a 4-conductor phone cord?

The LCD will show values for Volts, Amps, Ahrs, etc, but the LED will not be active on the CM/R. 
It is recommended to use a 6-conductor phone cord for full functionality.
Was this helpful?
What can we do to improve the information ?