Technical FAQs

Ask a Question

What are the part numbers of the Bonding screws that are included with the QOM100VH (or QOM100VHCP) Main Breakers?

Issue:
Current design parts

Product Line:
QOM1 Main Circuit Breakers

Environment:
Bonding Screw

Cause:
Application

Resolution:
The QOM100VH(or QOM100VHCP) comes with two bonding screws one of them is part number 4028318561(this is a 10-32 x 1.06in.) and the other is part #4028345850 (this is a1/4-20 x 1.01in.)
Was this helpful?
What can we do to improve the information ?