Technical FAQs

Ask a Question

What is the difference between a XCSE7311MH00300 and a standard XCSE7311?

Issue:
What is the difference between a XCSE7311MH00300 and a standard XCSE7311?

Product Line:
Safety Limit Switches - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
The XCSE7311MH00300 is a standard XCSE7311 with a 12 pin connector.  This unit was never marketed in the US and was developed for a specific European customer, but this unit is orderable in the US.
Was this helpful?
What can we do to improve the information ?