Technical FAQs

Ask a Question

Can the 9003KAC1B be ordered with markings 1 – 8 at 45 degree angles?

Question
Can the 9003KAC1B be ordered with markings 1 – 8 at 45 degree angles?

Issue:
Can the 9003KAC1B be ordered with markings 1 – 8 at 45 degree angles?

Product Line:
Cam Switches

Environment:
30mm Push Button Operators

Cause:
Product Selection

Resolution:
Yes it can. It To order one of these bezel operators with a standard marking, add the code (found in the document below) of the desired marking as a suffix to the operator type number. Example: 9003 KAC1B 4-21.

 
Was this helpful?
What can we do to improve the information ?