Technical FAQs

Ask a Question

What are the repair parts for the EZM31200JCBT, Series M01 main circuit breaker unit?

Issue:
Current design repair parts

Product Line:
EZM Metering Equipment

Environment:
repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:

Top Cover - 7329386378 (the top cover includes the handle)
Bottom Cover - EZM31200JCBTBC (the bottom cover includes all the labels, the handle, the breaker box/cover  and latch)
Main Breaker - PJM36120U31A 
Cover Screws - 4020513002K (This is a pack of 10 screws)
Cover Sealing Screw - X1299 (Top cover requires 2) 
Bonding Strap Kit - 7329696760 
Mounting Channel -  7329354303
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 
VISI-TITE NUT/WASHER - 7329697350 (this is the Double Deaded nut with the RED disc, that is used to tighten the Main Horizontal Cross Bus together)

 
Was this helpful?
What can we do to improve the information ?