Technical FAQs

Ask a Question

Can the NEMA 7/9 9001BR Control Stations come with a top entry for conduit?

Issue:
Can the NEMA 7/9 Control Stations come with a top entry for conduit?

Product Line:
9001BR Control Stations- GIC Product

Environment:
US Product

Cause:
Product Selection

Resolution:
The 9001BR Stations come standard with conduit entry at the bottom.  To adapt the control station for top entry, remove the cover of the unit, unscrew the internal switch, flip the internal switch around and remount inside the enclosure, flip the cover around and rescrew together.  The station will now have a top mount for the conduit.
 
Was this helpful?
What can we do to improve the information ?