Technical FAQs

Ask a Question

Can the HOM4284L225PRB load center, a main lugs load center, be converted to a main breaker load center?

Issue:
Product feature

Product Line:
Homeline Load Center

Cause:
Clarification of product feature

Resolution:
Yes, this load center is a convertible main that accepts QOM2 main breaker kits, 225A maximum.
Was this helpful?
What can we do to improve the information ?