Technical FAQs

Ask a Question

What are the repair parts for the EZM11200JCBE, Series M01 main circuit breaker unit?

Current design repair parts

Product Line:
EZM Metering Equipment

repair parts


Only the parts listed below are considered field replaceable:

Top Cover - EZM11200JCBETC (the top cover includes the handles, breaker box/cover and all appropriate labels)
Bottom Cover - 7329386385 (the bottom cover includes the handles)
Main Breaker - PJF36120U31A
Cover Screws - 4020513002K (This is a pack of 10 screws)
Cover Sealing Screw - X1299 (Top cover requires 2 and the bottom cover requires 2) 
Bonding Strap Kit - 7329696759 
Mounting Channel - 7329354306
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 
VISI-TITE NUT/WASHER - 7329697350 (this is the Double Deaded nut with the RED disc, that is used to tighten the Main Horizontal Cross Bus together)
Was this helpful?
What can we do to improve the information ?