Technical FAQs

Ask a Question

What is the function of T/k button for ATV71?

When the T/k button is active, this will mean the graphic display terminal will override the channels for the speed reference & the drive will take its speed ref. from the graphic display terminal regardless the channels configuration
If T/K is not active, this means the drive will use the reference channels that are configured, where you can chose a main channel & another channel & decide a parameter or logic input,,,etc to switch between them.
Was this helpful?
What can we do to improve the information ?