Technical FAQs

Ask a Question

What type fuses does the QMB326W or QMB366W accept?


Product Line:
QMB Fusible Branch Switches

Application of fuses 

The QMB326W and QMB366W switches will accept a Class H or K fuses as standard, Class R or J fuses with field modification. When using Class R fuses, also purchase and install Class R Fuse Kit QMB4060R, which when installed will reject all but Class R fuses. To convert the QMB326W or QMB366W for use with Class J fuses, relocate the load base assemblies and insulators to the mounting location nearest the line base assemblies. This information is located on the switch wiring diagram
Was this helpful?
What can we do to improve the information ?