Technical FAQs

Ask a Question

What is the part number for the protection tube for a XUSL4E30H106N light curtain?

Issue:
What is the part number for the NEMA 4X protection tube for a XUSL4E30H106N light curtain?

Environment:
Light Curtain,  XUSL, IP69K

Cause:
Need NEMA 4X or greater protection tube for XUSL4E30H106N light curtain being used in a food environment.

Resolution:
 The protection tube for the XUSL4E30H106N light curtain is XUSL4E30H106LWC, it is IP69K rated.
 
Was this helpful?
What can we do to improve the information ?