Technical FAQs

Ask a Question

What are the repair parts for the EZM11600JCBC Series M01 Main device?

Issue:
Current design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:

Top Cover assembly - 7329386452 (cover assembly includes the handles, the breaker door, the latches and all appropriate labels)
Bottom cover assembly - 7329695959 (cover assembly includes handles and latch) 
Cover Screws - 4020513002K (this is a bag of 10 cover screws and each cover uses 4 screws)
Main Circuit Breaker - RJF36160U31A
Main Lug - 4025113650 (There are six lugs per phase and neutral for a total of 18 main lugs)
Main lug mounting bolt - 2271028560 (requires one per lug)
Main lug mounting Nut - 2342702800 (requires one per lug)
Bonding Strap Kit  - 7329696757 
Mounting Channel - 7329654302
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 
Main Horizontal Bus 'VISI-TITE' Nut - 7329697350 (This is the Double headed nut with the Red disc that connects the main horizontal bus from one EZM unit to the next)
Was this helpful?
What can we do to improve the information ?