Technical FAQs

Ask a Question

What are the repair parts for the EZM11200JCBU Series M01 Main device?

Current design repair parts

Product Line:
EZM Metering

Repair parts


Only the parts listed below are considered field replaceable:

Top Cover assembly - EZM11200JCBUTC (cover assembly includes the handles, breaker door/box and all appropriate labels)
Bottom cover assembly - 7329386381 (cover assembly includes handle and latch) 
Cover Screws - 4020513001K (this is a bag of 10 cover screws)
Main Circuit Breaker - PJP36120U31A
Bonding Strap Kit  - 7329696760 
Mounting Channel - 7329354303
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 
Top cover Sealing Screws - X1299 (two required)
Main Horizontal Bus 'VISI-TITE' Nut - 7329697350 (This is the Double headed nut with the Red disc that connects the main horizontal bus from one EZM unit to the next)
Was this helpful?
What can we do to improve the information ?