Technical FAQs

Ask a Question

Can you order just the side rails for Trench Duct?

Issue:
Can you order just the side rails for Trench Duct?

Product Line:
Wire Management/Trench Duct

Environment:
Application

Cause:
Only rails and covers required

Resolution:
Yes the RS120 is a 10' long side rail that has an adjustable 2 3/8- 3 3/8" Height adjustment . P/N RS120-3 is for the 3"- 4"Height adjustable rails. Qty 2 required , one for left side and one for right side 
Was this helpful?
What can we do to improve the information ?