Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H321N, Series F05 (F5) Heavy Duty safety switch?

Issue:
Lug wire range

Product Line:
Heavy Duty Safety Switch

Environment:
30A HD Switches

Cause:
Clarification

Resolution:
The lugs installed in this switch will accept (1) #14 AWG - #2 AWG or (2) #14 AWG - #10 AWG aluminum or copper conductors. However, the wire bending space available in the switch restricts the conductors to (1) #14 AWG - #6 AWG or (2) #14 AWG - #10 AWG copper or aluminum conductors per phase.



CTA-ID : 2052198
Was this helpful?
What can we do to improve the information ?