Technical FAQs

Ask a Question

What is the quantity and size of wire that can be terminated on the DT400N Neutral Assembly?

Issue:
Product Features

Product Line:
Double Throw Safety Switch

Cause:
Clarification of wire range

Resolution:
The DT400N Neutral Assembly is provided with (3) lugs with a wire range of (1) #1/0 AWG - 750 KCMIL or (2) #1/0 AWG - 300 KCMIL AL/CU wires per lug for the incoming and outgoing neutral wires and (2) lugs with a wire range of #6 AWG - 300 KCMIL AL/CU for service ground(s).

CTA-ID : 2049028
Was this helpful?
What can we do to improve the information ?