Technical FAQs

Ask a Question

What gauge of steel is used for the HOM40M200CVP?

Issue:
Product characteristics

Product Line:
Homeline Load Center

Cause:
Clarification of metal thickness

Resolution:
The cover and the enclosure are manufactured from 16 gauge steel. 
Was this helpful?
What can we do to improve the information ?