Technical FAQs

Ask a Question

What is the replacement module for an TVS4IMA48B or TVS4IMA48BC?

Issue:
Question:
What is the replacement phase modules for the TVS4IMA48B TVS4IMA48BC?

Product Line:
Surge Protective Device (SPD), Surgelogic, NQ/NF panel

Environment:
Maintenance/Replacement

Cause:
Need to replace the phase modules on a surge protection device.

Resolution:
Use MA4IMA24 - two per phase, replace both. 
:
" C " in part number indicates that there is a surge counter on the display module.
Was this helpful?
What can we do to improve the information ?