Technical FAQs

Ask a Question

Can we install NQ 14 inch interiors and covers to match existing boxes?

Issue:
Can we install NQ 14 inch interiors and covers to match existing boxes 

Produce Line:
14" wide NQ panelboards

Environment:
Retrofit

Cause:
Difficulty or impossibility of changing out existing box

Resolution:
When the box is 14" wide, we have to provide them with 14" wide interiors (Digest page 9-8).
On these interiors, the existing boxes can not be any more than 1.5" shorter than our standard
box height for the interior to fit. The interiors are supplied as RTI and the special trims
are placed on separate line items and forced to Peru.
 
Was this helpful?
What can we do to improve the information ?