Technical FAQs

Ask a Question

What are the repair parts for the EZM31200GCBE Series M01 Main device?

Issue:
Current design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Top Cover assembly - EZM31200GCBETC (cover assembly includes the handles, breaker door/box and all appropriate labels)
Bottom cover assembly - 7329386385 (cover assembly includes handles) 
Cover Screws - 4020513002K (this is a bag of 10 cover screws)
Cover Sealing Screw - X1299
Main Circuit Breaker - PGF36120U31A
Bonding Strap Kit  - 7329696759 
Mounting Channel - 7329354306
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 


NOTE: THIS EZM MAIN IS DESIGNED FOR USE IN EUSERC UTILITY AREAS and DOES NOT COME STANDARD WITH LUGS. But comes standard with NEMA PADS, for MAIN LUGS see CAD drawing #PWFDS-SYTI-0030 in the 2D Cad system on-line)

Main lug mounting NUTS - 2342702800 (1/2-13 keps nut and they come standard on the device from the factory, there is one NUT per Stud and two nuts required per MAIN LUG)
Was this helpful?
What can we do to improve the information ?