Technical FAQs

Ask a Question

What are the repair parts for the EZM31600JCBC Series M01 Main device?

Issue:
Current design repair parts

Product Line:
EZM Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:

Only the parts listed below are considered field replaceable:
Top Cover assembly - 7329386453 (cover assembly includes the handles, latch, breaker cover door and all appropriate labels)
Bottom cover assembly - 7329695959 (cover assembly includes handles and latch) 
Cover Screws - 4020513002K (this is a bag of 10 cover screws, the top cover uses 4 and the bottom cover uses 4)
Main Circuit Breaker - RJF36160U31A
Standard Main and Neutral Lugs - 4025113650 (There are 6 lugs per phase and Neutral for a total of 24 lugs per device)
Main lug mounting hardware - 2271028560 (Bolt - 1/2-13 x 1.75" One Per Lug) AND 2342702800 (Nut - 1/2-13 keps nut, One per Lug)
Bonding Strap Kit  - 7329696757 
Mounting Channel - 7329654302
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP 

NOTE: For any alternate lugs see CAD drawing #PWFDS-SYTI-0007 in the 2D Cad system on-line)
Was this helpful?
What can we do to improve the information ?