Technical FAQs

Ask a Question

What is the replacement A, B and C phase module for the HL2IMA24C1?

Issue:
What is the replacement A,  B and C phase module for the HL2IMA24C1, Type 1 modules, 240kA,  120/208V, 3 phase, 4 wire, TVSS unit?

Product Line:
Surgelogic SPD BDG

Environment:
TVSS units sold and supported in the USA.

Cause: 
Maintenance/replacement TVSS module.

Resolution:
The replacement A,B and C phase module is MA1IMA241, (order one for each phase.)

Key Words:
TVSS,  phase modules, A, B and c replacements.
Was this helpful?
What can we do to improve the information ?