Technical FAQs

Ask a Question

Will the Homeline 2-pole, 50amp breaker, part number HOM250CP fit into the load center HOM24L70SCP?

Issue:
Product Features

Product Line:
Homeline Load Centers

Environment:
Branch Breakers

Cause:
Application 

Resolution:
Yes. The HOM250CP is a standard 2-pole, 50amp HOM branch breaker and the suffix 'CP' is only for Consumer packaging used in Retail. So it can be installed in the load center HOM24L70SCP, but will require both pole spaces.
Was this helpful?
What can we do to improve the information ?