Technical FAQs

Ask a Question

Are the 2 and 4 pole LC1D Contactors rated for inductive loads ?

Issue:
Are the 2 and 4 pole LC1D Contactors rated for inductive loads ?

Product Line:
D Line Contactor

Environment:
Application

Cause:
Clarification

Resolution: 
Yes, but due to the infrequent use of 2 pole and 4 pole contactors for motor loads, the Contactors are not shown with inductive ratings , but can be used for motor, or inductive loads nonetheless
Was this helpful?
What can we do to improve the information ?