Technical FAQs

Ask a Question

What ground bar(s) can be used in the load center HOM4080M200PC?

Issue:
Product Accessories  

Product line: 
Homeline load centers

Environement: 
Ground bars

Cause:
Application

Resolution: 
The wiring diagram for this load center will state "PK9 - 27GTA(L)". So any of the PK ground bars from the 9 hole(PK9GTA) up to the 27 hole(PK27GTA) can be used in this load center. Probably the more standard ground bar would be either the PK23GTA(23 holes) or PK27GTA (27 holes).

NOTE: The load center has 3 different mounting locations for the PK ground bars within the load center and each location is marked by a Ground bar symbol STAMPED in the box.
Was this helpful?
What can we do to improve the information ?