Technical FAQs

Ask a Question

Can the ATV21 / ATV212 series drive record date and time of a fault occurance?

Issue:
Can the ATV21 / ATV212 series drive record date and time of fault occurance?
 
Product Line:
Altivar 21 and Altivar 212 series drives.
 
Environment:
All models, All serial numbers.
 
Cause:
Customer needs the ability to record date and time of fault events.
 
Resolution:
The ATV21 / ATV212 series drives do not have the capability to record date and/or time of fault events.   The Altivar 61 / Altivar 71 series drives, equipped with an optional CIC card or IMC card can provided date and time stamping of events.






 
Was this helpful?
What can we do to improve the information ?