Technical FAQs

Ask a Question

Are fuse adapters available for fusible disconnect switches?

Issue:
Are fuse adapters available for fusible disconnect switches?

Product Line:
GS1/GS2 IEC Disconnect switches - GIC Product

Environment:
US Product

Cause:
Accessories - Product Characteristics

Resolution:
No, there are no fuse adapters to use with these switches.  Class J fusible disconnects are only meant to be used with class J fuses, and class CC disconnects with CC fuses.
Was this helpful?
What can we do to improve the information ?