Technical FAQs

Ask a Question

What is the part number for the ground bar kit for HOM2448M125PC load center?

Load Center accessories

Product Line;
Homeline load centers

Ground bars


The load center wiring diagram will state "PK9 - 27GTA(L)" equipment ground bar kits. So any PK ground bar from 9 holes(PK9GTA) through 27 holes(PK27GTA can be used in this load center. The most common would probably be either the PK15GTA  or  PK23GTA.

NOTE: The load center has 3 different locations(left side, right side and bottom side of the interior) where ground bars can be mounted. Each location will be marked with ground symbol STAMPED into the box.
Was this helpful?
What can we do to improve the information ?