Technical FAQs

Ask a Question

What is the catalog number for a generator interlock kit for the Obsolete QO30M150 series G1 load center?

ISSUE:
What is the catalog number for a generator interlock kit for the Obsolete QO30M150 Series G1 load center?

PRODUCT LINE:
Load Center

ENVIRONMENT:
Applies to the QO2030M150 Series G1 'ONLY' QO load center

CAUSE:
Selection for a generator interlock kit for an Obsolete QO load center.   

RESOLUTION: The generator interlock kit part number QOCGK2 can be used for the QO30M150 Series G1 load center, BUT the Generator kit part number will NOT be shown on the labeling of this  load center and labeling CANNOT be obtained because the load center is old and obsolete.  
 
Was this helpful?
What can we do to improve the information ?