Technical FAQs

Ask a Question

What is the order-able part number for the lug 31168-032-01?

Issue:
What is the part number for lug 31168-032-01

Product Line:
IEC Contactor and Disconnect Lugs - GIC Product

Environment:
US Product

Cause:
Product Selection and Characteristics

Resolution:
The 31168-032-01 is not sold as a separate piece.  It can only be purchased as part of kit GS1AW506.
 
Was this helpful?
What can we do to improve the information ?