Technical FAQs

Ask a Question

Is the locating hook on a PQ ** busway plug field replaceable?

Issue:
Is the locating hook for installation on a PQ** busway plug field replaceable?

Product Line:
Nema busway and accessories sold and supported in the USA.

Environment:
Maintenance

Cause:
If the hook breaks off, is it field replaceable?

Resolution:
The locating hook on the PQ  busway plug  is riveted to the enclosure and is not field replaceable.  
 
Was this helpful?
What can we do to improve the information ?