Technical FAQs

Ask a Question

Can an EZM1600CB main device be supplied with a 500 ampere circuit breaker instead of the 600 ampere circuit breaker?<br />

Issue:
Product offer

Product Line:
EZM

Environment:
Product offer

Cause:
Alternate trip setting needed

Resolution:
Yes, by ordering an EZM1600CB500.


CTA-ID : 2004176
Was this helpful?
What can we do to improve the information ?