Technical FAQs

Ask a Question

Micrologic RSU revision 8.5.1

Product Line:
Micrologic RSU (Remote Setting Utility) rev 8.5.1

The attached file contains the  RSU rev 8.5.1 program
(1) Download the attached file
(2) Unzip
(3) Navigate to exe folder
(4) Open Micrologic RSU.exe to run the program
Was this helpful?
What can we do to improve the information ?