Technical FAQs

Ask a Question

What is a QO1PJ15, and how many come in the kit?

Produce Line:
Panelboards

Environment:
Applies to NQ panelboards and QOB breakers only

Resolution:
The QO1PJ15 is a safety feature for finger-safe factory-assembled NQ panelboards. Instead of bolting a QOB to the panelboard bus finger, this kit allows a QOB breaker to snap into the bus bars. Catalog number QO1PJ15 includes 15 jaws for QOB breakers. Look at instruction bulletin 80043-809-01 for more details.






 
Was this helpful?
What can we do to improve the information ?