Technical FAQs

Ask a Question

What is the heat loss for the ATS22C32S6U?

Issue:
What is the heat loss for the ATS22C32S6U?

Product Line:
ATS22

Environment:
ATS22C32

Cause:
N/A

Resolution:
Heat loss :
During starting @ 3.5 ICL (Nominal current of the softstart) : 3699 Watts

During Steady State at full load : 96 Watts
                                Electronics : 20 Watts
                  Shorting Contactors : 14 Watts                                                                  
                                         Fans :  20 Watts                    
                ---------------------------------------------
                Total at Steady State : 150 Watts
Was this helpful?
What can we do to improve the information ?