Technical FAQs

Ask a Question

What is the bus bar rating for the QO132M100 load center?

Issue:
Application

Product Line:
QO Load Center

Environment:
Application

Cause:
Verification of rating

Resolution:
The QO132M100 is labeled as 125A maximum. 
Was this helpful?
What can we do to improve the information ?