Technical FAQs

Ask a Question

Is the L600AWK Circuit Breaker Enclosure Service Entrance rated?

Issue:
Product design features

Product Line:
Circuit Breaker Enclosures

Environment:
Service Entrance Rating

Cause:
Application

Resolution:
Yes, the L600AWK enclosure is Suitable for use as Service Entrance when following what the NEC requires for Service Entrance Applications. The NEC would require the Neutral assembly be installed and bonded.
Note the below Solid Neutral Assembly's can be used for this enclosure. SEE either CAD drawing or wiring diagram for terminal sizes.
1) SN400LA = 100-400Amp
2) SNC400LX = 100-400amp
3) SNC800LX = 200-800Amp
4) SN1000MA = 200-1000Amp
Was this helpful?
What can we do to improve the information ?