Technical FAQs

Ask a Question

Can multiple motors be connected on a single D-Line overload ?

Issue:
Application for overload relay

Product Line:
IEC Starters

Environment:
LRD, LR*D, LR*F

Cause:
OL Protection

 

Resolution:
 
 
 
Using one OLR for multiple motors is not allowed per
Code 430-53  . Further loadside lugs are rated to accomodate a single cable.

 
 
 
 
.
Was this helpful?
What can we do to improve the information ?