Technical FAQs

Ask a Question

When do the contacts change state on a LUAC11 contact block?

Issue:
Contact state change on LUAC11.

Product Line:
TeSys U Accessories - GIC Product

Environment:
US Product

Cause:
These contact blocks are not pole state change contact blocks

Resolution:
The LUAC11 has two contacts, one NO and one NC.  The NO changes to NC on ready, run, and overload trip (remote/auto reset).  The NC changes to NO on short circuit trip and overload trip (manual reset).
Was this helpful?
What can we do to improve the information ?