Technical FAQs

Ask a Question

What is the service voltage for the TVS6HWA50X surge protection device?

Issue:
What is the service voltage for the TVS6HWA50X surge protection device?

Produce line:
HWA Surge Protection Device, TVSS

Environment:
Nema 4X, 50kA peek surge current rating per Phase, Delta

Cause:
Is the TVS6HWA50X a 240Delta system.

Resoultion:
The Service Voltage for the TVS6HWA50X is  240V Delta., 3 phase, 3 wire + ground,
Was this helpful?
What can we do to improve the information ?