Technical FAQs

Ask a Question

Is the Q23225NRB circuit breaker enclosure CSA Certified?

Issue:
Standards

Product Line:
CB Enclosure

Environment:
CSA 

Cause:
Verification

Resolution:
The Q23225NRB is UL Listed but not CSA Certified. A CSA Certified equivalant would be Q23225NRBC. CSA File # LL 89067. 

Was this helpful?
What can we do to improve the information ?