Technical FAQs

Ask a Question

Is there a single-phase input version of the ATV630 process drive available?

Issue:
Is there a single-phase input version of the ATV630 process drive available?

Product Line:
Altivar 630 Process drives

Environment:
All models, All serial numbers

Cause:
Customer only has single phase power available but would like to use a Process drive.

Resolution:
There is currently no option available to power a Process drive with single phase power.
 
Was this helpful?
What can we do to improve the information ?