Technical FAQs

Ask a Question

What is the pinout for ATV58 remote HMI keypad cable?

Issue:
What is the pinout for ATV58 remote HMI keypad cable?

Product Line:
ATV58, Altivar 58

Environment:
All

Cause:
To connect a keypad to the drive using a cable.

Resolution:
The pinout for ATV58 keypad connection is as follows:
Signal: DA, 0VDC, DB, +VC
ATV58 wiring respectively DB9 connectors: Pins 3 to 3, 4 to 4, 7 to 7, 6 to 6

 
Was this helpful?
What can we do to improve the information ?